Can the KE02 accept a square wave external clock reference?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can the KE02 accept a square wave external clock reference?

Jump to solution
2,718 Views
babbott
Contributor I

I'd like to use the KE02 with an external clock reference to drive the oscillator of the micro-controller. Can the KE02 accept a square wave external clock reference and if so,what are the voltage specifications?

Thank you.

Labels (1)
0 Kudos
Reply
1 Solution
4 Replies
2,635 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Brent,

Mark gave you the clock source frequency spec. Regarding the clock source voltage spec, it also complies with the digital imput voltage rule, the high logic voltage must be greater than 0.7*VDD, the low voltage must be less than 0.35*VDD.

Hope it can help you.

BR

Xiangjun Rong

2,635 Views
babbott
Contributor I

Thanks. My question is whether or not the shape (square or sine) matters in this application. I have an external clock attached to the EXTAL pin but I am wondering if it needs to be a square or sine wave (or maybe it doesn't matter)?

0 Kudos
Reply
2,635 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to the following figure in the MKE02P64M40F0SF0.pdf.

you can connect the clock source to the Extal pin, it is okay.

Hope it can help you.

BR

Xiangjun Rong

pastedImage_1.png