Can't transmit using UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't transmit using UART

ソリューションへジャンプ
2,841件の閲覧回数
juanignaciotroi
Contributor III

Hello. I am starting a new project in which I need to communicate via UART. (I am develping with FRDM-KE02) I have tried to use the ConsoleIO provided by Processor Experto and used just the instruction "printf", I can't see any pulse train in my osciloscope when watch de PTA3 pin (Tx) in it.

I attatch the images of the configuration:

Captura de pantalla 2016-02-03 17.07.46.pngCaptura de pantalla 2016-02-03 17.07.40.pngCaptura de pantalla 2016-02-03 17.07.25.png

Thank you very much

タグ(2)
0 件の賞賛
返信
1 解決策
2,560件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Juan Ignacio Troisi:

There are some similar questions in the community:

Cannot toggle over PTA3 in FRDM-KE02Z

UART0 not working with KE06

UART0 not working with KE06

So the pins are true Open-Drain outputs.. External pull-ups are required to get a UART signal.


Best Regards!
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,561件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Juan Ignacio Troisi:

There are some similar questions in the community:

Cannot toggle over PTA3 in FRDM-KE02Z

UART0 not working with KE06

UART0 not working with KE06

So the pins are true Open-Drain outputs.. External pull-ups are required to get a UART signal.


Best Regards!
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,560件の閲覧回数
juanignaciotroi
Contributor III

Hello. Thank you for your help but I couldn't solve this problem yet. As adding pull up resistors didnt work, I have tried by configuring an AS component so that UART0 is asociated to pins PTB0 and PTB1. However, I still can't see anything different to 0V when trying to watch the Tx pin in my oscilloscope.

Here is a link with my project: Dropbox - asin ​. Maybe there is an error in software which I didnt detect.

Thank you very much

Juan Ignacio

0 件の賞賛
返信
2,560件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Juan Ignacio:

Sorry I just noticed that in FRDM-KE02 there is something else to consider. If you are measuring in the header pins then in the schematics you can see that there are some resistors not populated by default:

pastedImage_2.png

So to watch any of these signals on the header you need to solder 0 ohm resistors or simple solder joints, as well as removing the alternative function 0 ohm resistor.

Regards!

Jorge Gonzalez

0 件の賞賛
返信