Can't find I2S MCLK source options in K22F documentation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can't find I2S MCLK source options in K22F documentation

跳至解决方案
1,745 次查看
scottm
Senior Contributor II

The MK22FN1M0AVLH12 reference manual's section on the I2S module master clock says to see the chip-specific configuration information for the definitions of the input options used by I2Sx_TCR2[MSEL] and I2Sx_MCR[MICS].  I can't find those definitions in the chip-specific information - just the rather unhelpful statement that "The MCLK Input Clock Select bit of the MCLK Control Register (MCR[MICS]) selects the clock input to the I2S/SAI module’s MCLK divider."

Where are these clock source options listed?

Thanks,

Scott

标签 (1)
0 项奖励
回复
1 解答
1,623 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Scott,

See the chapter '5.7.9 I2S/SAI clocking' in K22P64M120SF5V2RM.

5.7.9 I2S SAI clocking.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,624 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Scott,

See the chapter '5.7.9 I2S/SAI clocking' in K22P64M120SF5V2RM.

5.7.9 I2S SAI clocking.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,623 次查看
scottm
Senior Contributor II

Thanks.  I was confused because 3.9.6.2 is also entitled "I2S/SAI clocking" and there's no indication there that more information is to be found elsewhere.  It would be great if someday all of the reference manuals had hyperlinks between sections whenever the relevant information is spread out.

Scott

0 项奖励
回复