Can Not Register While Using MSCAN_KEA_DEVD Driver For Test

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can Not Register While Using MSCAN_KEA_DEVD Driver For Test

2,030 次查看
brightwang
Contributor III

I'm Using MSCAN_KEA_DEVD Driver For My Kineties EA Projects Upon TRKEA128  Board. While Testing Load Balance I Find Something Error With MCU Reg. When I Get A Bytestream With Data Field Full Of 00 / 0XFF The Receving Thread Will Be Stuck In. No In-coming Message Will Changes The Reg But A Working Counter Here . It Is To Say I Cannot Read Any Update In Reg But Counter Is Still Working:

MSCAN_CANCTL0 0x98 0x40024000
MSCAN_CANCTL1 0xc4 0x40024001
MSCAN_CANBTR0 0x01 0x40024002
MSCAN_CANBTR1 0xdc 0x40024003
MSCAN_CANRFLG 0x00 0x40024004
MSCAN_CANRIER 0xff 0x40024005
MSCAN_CANTFLG 0x07 0x40024006
MSCAN_CANTIER 0x00 0x40024007
MSCAN_CANTARQ 0x00 0x40024008
MSCAN_CANTAAK 0x00 0x40024009
MSCAN_CANTBSEL 0x02 0x4002400a
MSCAN_CANIDAC 0x00 0x4002400b
MSCAN_CANMISC 0x00 0x4002400d
MSCAN_CANRXERR 0x1f 0x4002400e
MSCAN_CANTXERR 0x00 0x4002400f

Does Anyone Has Same Problem?

0 项奖励
回复
2 回复数

1,791 次查看
brightwang
Contributor III

Does Anyone Here Meet With The Same Problems With RX Register When Getting 00 00 00 00 00 00 00 00 Data Field?

0 项奖励
回复

1,791 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

I do a test with TRK-KEA128 board with MSCAN driver and could get CAN data frame: 00 00 00 00 00 00 00 00 with <Demo_Receive_DataFrame>.

In <main.c> file using below code:

    TEST_CASE_FUNC(Demo_Receive_DataFrame);

Please check below test result:

pastedImage_1.png

The MSCAN module registers value below:

pastedImage_2.png

pastedImage_3.png


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复