Can KV10 apply to use single shunt current sensing for BLDC Motor driver?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can KV10 apply to use single shunt current sensing for BLDC Motor driver?

1,675 次查看
Childe
Contributor II

I cannot find application note about single shunt current sensing for BLDC driver by using Kinetis V serie

标签 (1)
0 项奖励
回复
2 回复数

1,463 次查看
Childe
Contributor II

Thank you xiangjun.rong.

0 项奖励
回复

1,463 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Wittawas,

Regarding your question, I see that you would like to insert a shunt resistor or the other current sensor to measure the DC bus current, and use the current loop as the internal loop. Unfortunately, for BLDC motor control, we have the solution to use only speed loop, the speed loop output via PI or PID algorithms will change the duty cycle of PWM directly in about 1mS cycle time and drive MOSFET/IGBT directly to change the impressed voltage on the motor. We have not the solution to use speed loop as outer loop, use current loop as internal loop. In dual loop solution, the speed loop output via PID/PI is the  input current  reference for current loop, after we get the actual current spec via shunt resistor, compute the error between the input current  reference and the actual current, figure out the duty cycle of PWM signal via current PI/PID based on the error and drive MOSFET/IGBT in about 1mS cycle time.

In conclusion, from hardware, connect the shunt resistor to the DC bus between GND and node of 3 branches, let ADC sample the resistor voltage at the center of PWM signal, the FTM has 8 channels, you can use one FTM channel( which do not generate PWM) to set the sampling instant to implement the ADC sampling at the center of PWM signal. From software, the outloop is the speed loop, which can output the reference spec for the current loop, use the current loop as internal loop, whose output is the duty cycle time of PWM.

I suggest you refer to an1931, which uses FOC algorithms to control PMSM, but it uses both speed and current loop and use shunt resistor.

pls download an1931 from the website:

http://tinyurl.com/n5lzwyz

BR

XiangJun Rong