Can KEIL work with IAR J-Link Lite for Cortex-M debug probe?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can KEIL work with IAR J-Link Lite for Cortex-M debug probe?

ソリューションへジャンプ
6,424件の閲覧回数
BasePointer
Contributor II

Hi,

 

I want to order tower K60 from IAR. They will provide an IAR J-Link Lite for Cortex-M debug probe.

At the same time, I would like to evaluate KEIL. Can I use same debugger from IAR for also KEIL?

 

Thanks.

 

0 件の賞賛
返信
1 解決策
5,514件の閲覧回数
lukas
Contributor III

it doesnt support IAR J-link - when you try to download program - it detect the IAR tool, give back negative message and doest continue with the download

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
5,514件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

Keil uVision4 supports the J-Link / J-Trace from Segger. The IAR J-Link Lite is a low speed J-Link from Segger with IAR branding (but fast enough for most work).

 

Keil uVision4 (lastest version) also supports the inbuilt OSJTAG interface (as do all IDEs with Kinetis support) so will work without any external debugger.

 

Regards

 

Mark

 

0 件の賞賛
返信
5,514件の閲覧回数
BasePointer
Contributor II

Do you know that Keil also supports IAR J-Link Lite?

0 件の賞賛
返信
5,515件の閲覧回数
lukas
Contributor III

it doesnt support IAR J-link - when you try to download program - it detect the IAR tool, give back negative message and doest continue with the download

0 件の賞賛
返信
5,514件の閲覧回数
BasePointer
Contributor II

 

Thanks Lukas for this feedback.

0 件の賞賛
返信
5,514件の閲覧回数
mjbcswitzerland
Specialist V

Hi Lukas

 

Interesting. This sounds as though uVision is actively rejecting the J-Link with IAR branding since other programs don't seem to care whether it is a high speed J-Link, low speed J-Link or an IAR packaged one of these.

 

Regards

 

Mark

 

P.S. I'll have a try with an old IAR J-Link Lite once I get back from holiday....

0 件の賞賛
返信
5,514件の閲覧回数
DistiCasMgr
NXP Employee
NXP Employee

Hi,

 

I asked ARM about this today and was told the following:-

 

If the J-Link in question is branded as Segger it will work, if it is branded as IAR, then the embedded IAR firmware stops it from working with Keil MDK.  (So MDK is capable of using it  but IAR won’t let it happen...).

 

Hope that clarifies.

 

Damian

0 件の賞賛
返信