Can K21 USBDCD use for detect VBUS status?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can K21 USBDCD use for detect VBUS status?

Jump to solution
1,009 Views
jimyang
Contributor II

Hi,

Anybody tell me if K21 USBDCD can use for detect VBUS status? And how to do?

Thanks!

Jim

Labels (1)
0 Kudos
Reply
1 Solution
886 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Jim Yang

We recommend to use a GPIO pin as VBUS detection, which also could wake up the chip from all low power mode (includes LLS mode or VLLSx mode (using LLWU module with external pin)).

 

The VBUS connects to VREGIN and a GPIO pin doesn't cause conflict. I think customer can fly a wise to connect VBUS with related GPIO pin.


Hope this information helps you
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
887 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Jim Yang

We recommend to use a GPIO pin as VBUS detection, which also could wake up the chip from all low power mode (includes LLS mode or VLLSx mode (using LLWU module with external pin)).

 

The VBUS connects to VREGIN and a GPIO pin doesn't cause conflict. I think customer can fly a wise to connect VBUS with related GPIO pin.


Hope this information helps you
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply