Can I use raspberry pi for video processing and use the required output as a command to FRDM-K64F microcontroller?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I use raspberry pi for video processing and use the required output as a command to FRDM-K64F microcontroller?

1,380件の閲覧回数
balajiv
Contributor II

I want to process the traffic signs using open computer vision.Since raspberry pi is fast in image processing,will I be able to interface raspberry pi with FRDM-K64F microcontroller ?

ラベル(2)
0 件の賞賛
返信
1 返信

1,281件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

 There isn't offical reference design on how to connect FRDM-K64F with raspberry pi. But I think it is not a hard job. Both borads have plenty of interface, I2C,SPI, UART, USB, CAN... So it is depend on your usage.

Regards

Jing 

0 件の賞賛
返信