Can ADC pin be used an digital output pin?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can ADC pin be used an digital output pin?

跳至解决方案
2,601 次查看
Embionics
Contributor III

I am using MK60DN512VLL10 controller in our project.

By mistake, Instead of using port pin as digital output pin, I have used adc pin. 

Now is there any possible way to use the adc pin as digital IO pin

kindly refer to the below attachments (schematics)

标记 (1)
0 项奖励
回复
1 解答
2,437 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Amreen,

I am sorry, but ADC1_DM1 pin of K60 can only be used as ADC function, so you might have to connect another pin to the circuit by flying wire. Sorry for the inconvenience that might cause.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,438 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Amreen,

I am sorry, but ADC1_DM1 pin of K60 can only be used as ADC function, so you might have to connect another pin to the circuit by flying wire. Sorry for the inconvenience that might cause.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复