Can ADC pin be used an digital output pin?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can ADC pin be used an digital output pin?

ソリューションへジャンプ
2,556件の閲覧回数
Embionics
Contributor III

I am using MK60DN512VLL10 controller in our project.

By mistake, Instead of using port pin as digital output pin, I have used adc pin. 

Now is there any possible way to use the adc pin as digital IO pin

kindly refer to the below attachments (schematics)

タグ(1)
0 件の賞賛
返信
1 解決策
2,392件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Amreen,

I am sorry, but ADC1_DM1 pin of K60 can only be used as ADC function, so you might have to connect another pin to the circuit by flying wire. Sorry for the inconvenience that might cause.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,393件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Amreen,

I am sorry, but ADC1_DM1 pin of K60 can only be used as ADC function, so you might have to connect another pin to the circuit by flying wire. Sorry for the inconvenience that might cause.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信