CMSIS header files

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CMSIS header files

跳至解决方案
3,263 次查看
awilhelm
Contributor II

Are CMSIS headers available for all devices/families?

I'm specifically looking for MK22FN1M0VLL12.  I have KSDK 1.1.0, and have looked at the included devices; the closest I find is MK22F51212.

Is the KSDK the only place to find the CMSIS headers, or is there some other place to look?

Thanks.

标签 (1)
0 项奖励
回复
1 解答
2,727 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Andy Wilhelm:

Is the attached file what you need?

If you install KDS the CMSIS headers are available at the next installation path:

C:\Freescale\KDS_2.0.0\eclipse\ProcessorExpert\Config\PE\CPE\wizard_data\wizards\kds


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,728 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Andy Wilhelm:

Is the attached file what you need?

If you install KDS the CMSIS headers are available at the next installation path:

C:\Freescale\KDS_2.0.0\eclipse\ProcessorExpert\Config\PE\CPE\wizard_data\wizards\kds


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,727 次查看
qiangliu
Contributor I

by the way,where could we download such this file with other device,such as MKL16Z256,thank you!

0 项奖励
回复
2,727 次查看
awilhelm
Contributor II

Yes, that's the file I need.

Thanks.

0 项奖励
回复