CMSIS header files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,182件の閲覧回数
awilhelm
Contributor II

Are CMSIS headers available for all devices/families?

I'm specifically looking for MK22FN1M0VLL12.  I have KSDK 1.1.0, and have looked at the included devices; the closest I find is MK22F51212.

Is the KSDK the only place to find the CMSIS headers, or is there some other place to look?

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,646件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Andy Wilhelm:

Is the attached file what you need?

If you install KDS the CMSIS headers are available at the next installation path:

C:\Freescale\KDS_2.0.0\eclipse\ProcessorExpert\Config\PE\CPE\wizard_data\wizards\kds


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,647件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Andy Wilhelm:

Is the attached file what you need?

If you install KDS the CMSIS headers are available at the next installation path:

C:\Freescale\KDS_2.0.0\eclipse\ProcessorExpert\Config\PE\CPE\wizard_data\wizards\kds


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,646件の閲覧回数
qiangliu
Contributor I

by the way,where could we download such this file with other device,such as MKL16Z256,thank you!

0 件の賞賛
返信
2,646件の閲覧回数
awilhelm
Contributor II

Yes, that's the file I need.

Thanks.

0 件の賞賛
返信