CAN functionality in TWR-K21F120M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN functionality in TWR-K21F120M

1,079 Views
pratiekbhadrana
Contributor III

Hello,

Does the TWR-K21F120M have CAN functionality? It is not mentioned in the quick start guide or the user manual. But the K21 chip with 120MHz has CAN in its datasheet. So does the tower board have CAN or not?

Also, I am planning to buy a tower board or the first time. What is the difference between OSJTAG and OpenSDA on the FRDM boards ?

Do I have to buy the Elevator module also to use the tower module?

Thanks

0 Kudos
Reply
1 Reply

968 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Pratiek Bhadranavar:

Yes, the TWR-K21F120M has a K21FN1M0 part, which has CAN module integrated.

If you are planning on using CAN, then the Tower System (TWR-K21F120M + TWR-SER + TWR-ELEV) would be very useful, since the TWR-SER board has a CAN transceiver embedded.

Regarding OSBDM and OpenSDA, please check the answer provided by colleague Erich Styger in the next discussion:

What is difference between OpenSDA and OSBDM?

:smileyinfo: Just notice that Erich was talking about OpenSDAv1. But now there is version OpenSDAv2 which is open source. For details check the next document in community by colleague Anthony Huereca:

OpenSDAv2


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply