Redistribution license of the Kinetis K20 CMISIS headers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Redistribution license of the Kinetis K20 CMISIS headers

1,524件の閲覧回数
finnwilke
Contributor I

Hello,

In the Keil download are header files like MK20D5.h, MK20D10.h etc. which are the CMSIS compliant headers for the K20 platform. Is it allowed to redistribute these headers in an open source (LGPL) licensed project and if so, under which license are they allowed to be redistributed?

Thanks a lot

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,252件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

I recommend to ask KEIL support if that is allowed, since you downloaded the files from their site.


Hope this information can help you.

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,252件の閲覧回数
eicht
Contributor I

Hi,

I'd be also very much appreciate clarification of this topic. Does Freescale as copyright holder grant the right to redistribute these header files?

Thank you in advance.

Best wishes,

Thomas

0 件の賞賛
返信

1,252件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

You can redistribute the Freescale Header Files as long as you maintain the Freescale Copyright title:

/*

** ###################################################################

** Compilers: ARM Compiler

** Freescale C/C++ for Embedded ARM

** GNU C Compiler

** IAR ANSI C/C++ Compiler for ARM

**

** Reference manuals: K20P64M50SF0RM Rev. 1, Oct 2011

** K20P32M50SF0RM Rev. 1, Oct 2011

** K20P48M50SF0RM Rev. 1, Oct 2011

**

** Version: rev. 1.0, 2011-12-15

**

** Abstract:

** CMSIS Peripheral Access Layer for MK20D5

**

** Copyright: 1997 - 2011 Freescale Semiconductor, Inc. All Rights Reserved.

**

** http: www.freescale.com

** mail: support@freescale.com

**

** Revisions:

** - rev. 1.0 (2011-12-15)

** Initial version

**

** ###################################################################

*/

This is an example to demonstrates what I am referring with the Copyright title.


Hope this information can help you

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,252件の閲覧回数
finnwilke
Contributor I

Hi,

I contacted Keil support. They told me this:

The header files contain:

 Copyright: 1997 - 2012 Freescale Semiconductor, Inc. All Rights Reserved. 

This statement prohibits Keil to allow me anything and any questions regarding this must be answered by Freescale as they are the ones who own the Copyright.

Best wishes,

Finn Wilke

0 件の賞賛
返信