CAN as FLEXCAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
17,255件の閲覧回数
ivanrobles
Contributor III

Why is called CAN as FlexCAN? what is the difference?

ラベル(1)
1 解決策
9,022件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hi Ivan,

'Flexcan' is only the name of the IP module. We have in Freescale several CAN controllers in different MCU families, MSCAN, FLEXCAN,....Every CAN controller have different features in terms of buffers, FIFO's, mailboxes, etc.. The important thing is that module is compliant with CAN standards. From RM:

"The FlexCAN module is a communication controller implementing the CAN protocol according to the CAN 2.0B protocol specification"

If the module have additional features, you can manage the CAN bus with more flexibility and capabilities or less CPU load.

Luis

元の投稿で解決策を見る

3 返答(返信)
9,023件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hi Ivan,

'Flexcan' is only the name of the IP module. We have in Freescale several CAN controllers in different MCU families, MSCAN, FLEXCAN,....Every CAN controller have different features in terms of buffers, FIFO's, mailboxes, etc.. The important thing is that module is compliant with CAN standards. From RM:

"The FlexCAN module is a communication controller implementing the CAN protocol according to the CAN 2.0B protocol specification"

If the module have additional features, you can manage the CAN bus with more flexibility and capabilities or less CPU load.

Luis

6,204件の閲覧回数
JabezLaw
Contributor II
Thanks
0 件の賞賛
返信
9,022件の閲覧回数
ivanrobles
Contributor III

Thank you very much

0 件の賞賛
返信