CAN as FLEXCAN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CAN as FLEXCAN

跳至解决方案
17,250 次查看
ivanrobles
Contributor III

Why is called CAN as FlexCAN? what is the difference?

标签 (1)
1 解答
9,017 次查看
LuisCasado
NXP Employee
NXP Employee

Hi Ivan,

'Flexcan' is only the name of the IP module. We have in Freescale several CAN controllers in different MCU families, MSCAN, FLEXCAN,....Every CAN controller have different features in terms of buffers, FIFO's, mailboxes, etc.. The important thing is that module is compliant with CAN standards. From RM:

"The FlexCAN module is a communication controller implementing the CAN protocol according to the CAN 2.0B protocol specification"

If the module have additional features, you can manage the CAN bus with more flexibility and capabilities or less CPU load.

Luis

在原帖中查看解决方案

3 回复数
9,018 次查看
LuisCasado
NXP Employee
NXP Employee

Hi Ivan,

'Flexcan' is only the name of the IP module. We have in Freescale several CAN controllers in different MCU families, MSCAN, FLEXCAN,....Every CAN controller have different features in terms of buffers, FIFO's, mailboxes, etc.. The important thing is that module is compliant with CAN standards. From RM:

"The FlexCAN module is a communication controller implementing the CAN protocol according to the CAN 2.0B protocol specification"

If the module have additional features, you can manage the CAN bus with more flexibility and capabilities or less CPU load.

Luis

6,199 次查看
JabezLaw
Contributor II
Thanks
0 项奖励
回复
9,017 次查看
ivanrobles
Contributor III

Thank you very much

0 项奖励
回复