CAN & RTC on K60 device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN & RTC on K60 device

2,718件の閲覧回数
anandsingh
Contributor I


Hi,

 

I am using K60 device in my project and facing issue on RTC and CAN module.

 

Please find the attached screen shot and code.Here I have tested individual module, but still I am not able to find the success.

 

I attached the snapshot also for your reference.

 

With RTC code it is terminated on the Debughault in debug perspective.

 

With CAN its showing CAN frame send success but still there is no activities on the CAN_Rx & CAN_Tx pin of controller.

 

Please tell us for the where I am committing the mistake.

 

Regards.

Anand

Original Attachment has been moved to: RTC_MODULE.rar

Original Attachment has been moved to: CAN_MODULE.rar

0 件の賞賛
返信
3 返答(返信)

2,609件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Anand,

When did the RTC issue happen? I notice there are three APIs called in that project, RTC1_Init(),RTC1_SetTime() and RTC1_GetTime(). Which one would cause Debughault issue? Please kindly help to clarify.

Thanks for your patience!!


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,609件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Anand,

Actually the RTC_MODULE runs well on my side, please kindly refer to the following for details. This demo run on a TWR-K60F120M, not sure the device on your side, would you please help to clarify? Thanks for your patience!!

result.png


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,609件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Anand,

Unfortunately, I can not open the CAN_MODULE by CW 10.5, would you please help to clarify?

error.png


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信