CAN Connection between a TWR-K60D100M and MIMXRT1064-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN Connection between a TWR-K60D100M and MIMXRT1064-EVK

Jump to solution
1,479 Views
Dannii
Contributor II

Hey guys,

when connecting the Boards togehter through their CAN Ports and using a Driver for the K60 both seem to work when checking it with an Oscilloscope, but when using the Flexcan example it seems to be not working. Maybe I would guess it is related to the Baudrate because in the exmaple they are on two different ones. But I probably need some help changing the baudrate and maybe other values to connect the devices. When using a TWR-K64 with the 1064 it works like it should but they are configured the same way in the example. 

Best regards

Daniel

0 Kudos
Reply
1 Solution
1,472 Views
Dannii
Contributor II

The Baudrate was the only problem and I fixed it by just changing it in the default settings. 

View solution in original post

1 Reply
1,473 Views
Dannii
Contributor II

The Baudrate was the only problem and I fixed it by just changing it in the default settings.