CAN Connection between a TWR-K60D100M and MIMXRT1064-EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CAN Connection between a TWR-K60D100M and MIMXRT1064-EVK

跳至解决方案
1,477 次查看
Dannii
Contributor II

Hey guys,

when connecting the Boards togehter through their CAN Ports and using a Driver for the K60 both seem to work when checking it with an Oscilloscope, but when using the Flexcan example it seems to be not working. Maybe I would guess it is related to the Baudrate because in the exmaple they are on two different ones. But I probably need some help changing the baudrate and maybe other values to connect the devices. When using a TWR-K64 with the 1064 it works like it should but they are configured the same way in the example. 

Best regards

Daniel

0 项奖励
回复
1 解答
1,470 次查看
Dannii
Contributor II

The Baudrate was the only problem and I fixed it by just changing it in the default settings. 

在原帖中查看解决方案

1 回复
1,471 次查看
Dannii
Contributor II

The Baudrate was the only problem and I fixed it by just changing it in the default settings.