Building Kinetis M bare metal examples!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Building Kinetis M bare metal examples!

1,728件の閲覧回数
frq03719
NXP Employee
NXP Employee

Good Morning,

I need a very simple help. Do you have a getting started document, that explains step by step how the build the bare metal examples in KDS 3.0.2. 

The only explanation i found is this one :

MKMxxZxxACxx5 Bare Metal Software Drivers: Introduction

CREATING NEW PROJECT
Execute make_project.exe script from the "template" subfolder to create a new project. The script creates a new project based on selected toolchain, debugger probe, device derivative and project name. The new project can be either standalone or part of drivers' installation. The standalone project will be created in a specific subfolder and it will contain snapshot of all source files necessary to build application.

Ok, I have a standalone project, but how to get it into KDS. It seems KDS 3.0.2 does not recognize any project.... 

0 件の賞賛
返信
1 返信

1,656件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Olivier,

I'm not sure why you need KDS3.0.2. The most update KDS is 3.2, nobody use 3.0.2. I haven't install it either. Since the steps of create a new project should be same. The attachment is KDS user guide. Please see or let customer see section 2.2. This file also can be found in KDS install directory.

KDS has many patch to compatible with new SDK and function. You can download them from Design Studio Integrated Development Environment (IDE) | NXP . The old version and patch is in the "previous" table.

Regards,

Jing

0 件の賞賛
返信