Bug in FRDM-KL27z Schematic?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bug in FRDM-KL27z Schematic?

1,230件の閲覧回数
bcstewart
Contributor III

According to the KL27 data sheet Rev 5, the MK27Z256VLH4 defines pin 8 as VREGIN.

pastedImage_2.png

But on the FRDM schematic (SPF-28303_B.pdf), pin 8 is used as an A/D input.  Furthermore, there appears to be no REGIN input at all (no 5V from USB).

pastedImage_3.png

Is this a bug?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,094件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi BC Stewart,

   No, no Bug in the FRDM-KL27Z schematic.

   You are referring to the wrong reference manual.

   Please note, the chip on FRDM-KL27 is:KL27Z64VLH4, you are referring to the 128K 256K KL27 chip, the correct RM for FRDM-KL27 is:

http://www.nxp.com/assets/documents/data/en/reference-manuals/KL27P64M48SF2RM.pdf 

pastedImage_3.png

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信