Hello,
If you need any specific inputs from me please as
Solved! Go to Solution.
1. Do I need to write code to bring up the micro controller ? (Hope I don't need to write. This micro controller have some software internally to start)
TS: The flash need be programed with customer application code. The flash memory is empty when chip shipped.
2. I may need to write like a device driver stuff to configure the external devices (LCD and the electrical sensor) right ?
TS: Yes, the LCD driver could refer TWR-KM34Z50M LCD demo and the sensor need to check which communication module using SPI/I2C, there already with SPI and I2C driver.
3. Is MQX Lite RTOS software need any code modification to support the chip MKM34Z128CLL5 / it requires some configurations ?
TS: There with configuration options as PE component.
4. For debugging this board is still OpenSDA is enough or do you have a better suggestion ?
TS: In general, customer could select to use P&E Multilink Universal or Segger J-Link debugger tool.
More detailed info, please check below link:
http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320137
http://www.segger.com/jlink-debug-probes.html
While, customer also could consider to use OpenSDA, as general debug application, that will be suitable.
Wish it helps.
best regards 
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
If customer is using TWR-KM34Z50M boardd? If yes, CodeWarrior MCU V10.6 and OpenSDA(debugger) is enough for the development.
Customer can download KM34 CodeWarrior example project from below link:
http://cache.freescale.com/files/32bit/software/TWR-KM34_DEMO_SW.zip
About RTOS, customer can consider to use MQX Lite, which is embedded in Processor Expert software (as a component).
CodeWarrior MCU v10.6 also with Processor Expert software.
Wish it helps.
best regards 
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ma Hui,
Thanks for your reply.
I will go through the project that you have suggested.
It is a custom board. we are not using TWR-KM34Z50M. This custom board has 1 LCD display and a electrical sensor chip.
We are using MKM34Z128CLL5.
Basically I need to configure this LCD display and the electrical sensor chip.
As I am very new to Micro controllers I need to understand the below things.
My questions are (May silly, but pls help me to understand),
1. Do I need to write code to bring up the micro controller ? (Hope I don't need to write. This micro controller have some software internally to start)
2. I may need to write like a device driver stuff to configure the external devices (LCD and the electrical sensor) right ?
3. Is MQX Lite RTOS software need any code modification to support the chip MKM34Z128CLL5 / it requires some configurations ?
4. For debugging this board is still OpenSDA is enough or do you have a better suggestion ?
thanks for your help again.
Regards,
Sivanesan R.
1. Do I need to write code to bring up the micro controller ? (Hope I don't need to write. This micro controller have some software internally to start)
TS: The flash need be programed with customer application code. The flash memory is empty when chip shipped.
2. I may need to write like a device driver stuff to configure the external devices (LCD and the electrical sensor) right ?
TS: Yes, the LCD driver could refer TWR-KM34Z50M LCD demo and the sensor need to check which communication module using SPI/I2C, there already with SPI and I2C driver.
3. Is MQX Lite RTOS software need any code modification to support the chip MKM34Z128CLL5 / it requires some configurations ?
TS: There with configuration options as PE component.
4. For debugging this board is still OpenSDA is enough or do you have a better suggestion ?
TS: In general, customer could select to use P&E Multilink Universal or Segger J-Link debugger tool.
More detailed info, please check below link:
http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320137
http://www.segger.com/jlink-debug-probes.html
While, customer also could consider to use OpenSDA, as general debug application, that will be suitable.
Wish it helps.
best regards 
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ma Hui,
Thanks for your answers and suggestions.
From your answers I have got a good understanding.
Regards,
Sivanesan R.
Hi Ma Hui,
Need one more clarification.
Will Segger's J-Link base work with Code warrior without any additional software ?
Or do I need buy any additional software from them to make the J-link base work with CW.
Regards,
Sivanesan R
CodeWarrior comes installed with all the needed Segger software and drivers, so you can use a Segger J-Link out of the box.
Some Segger units can have extra add-on features and licenses (like unlimited FLASH breakpoints), but this is handled directly by the Segger software.
You can downoad the latest Segger software/drivers from the Segger web site, and it will detect your CodeWarrior installation and update it as necessary.
Erich
Thank you Ma Hui and Erich !
Maybe you need to download J-Link driver from below link, I am not quite sure if CW already provides J-Link driver.
SEGGER - The Embedded Experts - Software
After J-Link driver installed, there no need other software any more.
Wish it helps.
best regards 
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------