Bootloader for kinetis k40

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bootloader for kinetis k40

3,040 次查看
mpc8377e
Contributor I

Hi,

 

Does the Tower module TWRK40X256 comes up with any bootloader? I need to use a bootloader on kinetis K40, is there any bootloader available for K40?

 

/Raghu

0 项奖励
回复
1 回复

1,605 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

 

K40 has not any bootloader, out of reset executes out of internal flash. You have the OSJTAG to program the device using CW, IAR, Keil,...

 

Regarding bootloaders for Kinetis:

 

 

AN4367 : Ethernet Bootloader for MCU (pdf)| AN4367SW |   
This document explains how to modify the .lcf and .icf link files of CodeWarrior and IAR IDEs respectively, in order to...

AN4370 : USB DFU Bootloader for MCUs (pdf)| AN4370SW |   
This document demonstrates how DFU fits in an embedded device and gives examples of implementation using a PC with...

AN4368 : USB Mass Storage Device Host Bootloader (pdf)| AN4368SW |   
Bootloader is a small program put into a device that allows user application codes to be programmed to the...

AN4379 : Freescale USB Mass Storage Device Bootloader (pdf)| AN4379SW |   
This application note describes a mass storage device (MSD) USB bootloader that has been written to work with...

 

Cehck also AN2295, serial bootloader:

 

https://community.freescale.com/message/97604#97604

 

 

Best Regards,

 

Luis

 

0 项奖励
回复