Boot pin for Kinetis MKL16Z128VLH4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot pin for Kinetis MKL16Z128VLH4

1,101 Views
arunkannan
Contributor III

Which is the boot pin for MKL16Z128VLH4 Kinetis KL16 MCU.

I can only see the reset pin in datasheet.

Are reset pin and boot pin the same?

Let us know which is the boot pin?

 

0 Kudos
Reply
1 Reply

1,067 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For the Kinetis KL16, there is not regular boot mode, I mean that you can not download application  binary to flash via uart, spi...for KL16.

The KL16 will execute code in flash directly after Reset, but you can write the 0x0_040D(Flash top address) so that you can configure the core clock, enable/disable the Reset pin and NMI pin...

For detailed inf, pls refer to section 27.3.1 Flash Configuration Field Description and section 6.3.2 FOPT boot options in the RM of Kl16.

In conclusion, there is Reset pin, there is not BOOT pin.

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply