Boot pin for Kinetis MKL16Z128VLH4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Boot pin for Kinetis MKL16Z128VLH4

1,045 次查看
arunkannan
Contributor III

Which is the boot pin for MKL16Z128VLH4 Kinetis KL16 MCU.

I can only see the reset pin in datasheet.

Are reset pin and boot pin the same?

Let us know which is the boot pin?

 

0 项奖励
回复
1 回复

1,011 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For the Kinetis KL16, there is not regular boot mode, I mean that you can not download application  binary to flash via uart, spi...for KL16.

The KL16 will execute code in flash directly after Reset, but you can write the 0x0_040D(Flash top address) so that you can configure the core clock, enable/disable the Reset pin and NMI pin...

For detailed inf, pls refer to section 27.3.1 Flash Configuration Field Description and section 6.3.2 FOPT boot options in the RM of Kl16.

In conclusion, there is Reset pin, there is not BOOT pin.

Hope it can help you

BR

XiangJun Rong

 

0 项奖励
回复