Beginner on KL15, where to begin?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Beginner on KL15, where to begin?

ソリューションへジャンプ
1,757件の閲覧回数
markosiponen
Contributor III

Hello

I have previously worked with STM32 (Cortex M3 from ST).

Now I must learn how to use an KL15. Where do I begin learning the KL15? Where can I find the best code examples and training material?

I have ordered a FRDM-KL25Z to start testing my code.

Is there a peripheral driver library available for this MCU? Or do I have to write all peripheral setup functions by myself (ST have a great peripheral driver library for their STM32 series)?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,523件の閲覧回数
vivacious
Contributor II

You may like to start with some sample codes done for you. (look for "KL25_SC.exe".....in the "download" tab for the board)

If you are on IAR...then it's lot better but not to worry even if you are CW.

Good luck!!

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,524件の閲覧回数
vivacious
Contributor II

You may like to start with some sample codes done for you. (look for "KL25_SC.exe".....in the "download" tab for the board)

If you are on IAR...then it's lot better but not to worry even if you are CW.

Good luck!!

0 件の賞賛
返信