Basic example code for twr-k20d72m evaluation board for KDS IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Basic example code for twr-k20d72m evaluation board for KDS IDE

1,479件の閲覧回数
parthmodi
Contributor I

Hi,

We purchased the twr-k20D72M evaluation board. We want to test all peripheral devices with the example code.

We get the example code from the below link, but all this examples code are only for the IAR and CW IDE.

Kinetis K20 72 MHz MCU Tower System Module|NXP

We are wok on the KDS IDE. We have below queries regarding same.So, we are requested to addressing them.

Queries,

1) Please share the basic example code and document for the KDS.

2) We need the GPIO,UART,SPI,I2C,I2s demo code for this evaluation board.

3) Please share a basic document for import this example code.

Thanks & regards,

Parth

0 件の賞賛
返信
1 返信

1,177件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Parth,

Please find attached 2 example projects for the TWR-K20D72M , GPIO and UART.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信