Are all analogs inputs compatible for 16-bit ADC mode on a MK10DX256VLL7 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are all analogs inputs compatible for 16-bit ADC mode on a MK10DX256VLL7 ?

848 Views
bathof
Contributor I

We would like to use 10 analogs input as 16-bits ADC mode.

After having read the chapter 6.6.1 of the datasheet K10P100M72SF1, we don't understand the specifications of the single-ended channels. Is it possible to use them with the 16-bit ADC mode.

Datasheet link : http://cache.freescale.com/files/32bit/doc/data_sheet/K10P100M72SF1.pdf?fasp=1&WT_TYPE=Data%20Sheets...

Best regards.

Labels (1)
0 Kudos
Reply
1 Reply

690 Views
mjbcswitzerland
Specialist V

Hi

All ADC inputs can be operatzed in 16 bit mode.

Note that a maximum of 4 ADC inputs can be sampled at a time by HW (using two AD-controllers in your device - each in hardware trigger mode using channels A and B), so to use more than these you will need to multiplex them in SW.

Regards

Mark

0 Kudos
Reply