Hi
Is anybody running MQX on a K60 processor with external SRAM?
Currently I am exhausting RAM, which manifests itself when TCP sockets are opened. Currently only have about 20K free when the application is running.
So the question is really how easy will it be to add external sram and make MQX aware/use it. (Also any idea if there is a performance hit?)
Regards
Gary
已解决! 转到解答。
Yes, I've done it. I'm the hardware guy, so I'm not up to speed with all the MQX issues, but basically we hung 1Mx16 SRAM on the Flexbus and used FB_CS3 to decode it. It works better if you don't mix up your BHE and BLE strobes. With 70nsec SRAM we needed 4 wait states with a 50MHz Flexbus clock, so there is a performance penalty. You haven't specified which K60 you are using as the subfamily 3 parts will cache the SRAM and the subfamily 2 parts wont.
I don't think the MQX bit was too difficult. I think you just need to edit your .icf and rebuild your BSP.
Yes, I've done it. I'm the hardware guy, so I'm not up to speed with all the MQX issues, but basically we hung 1Mx16 SRAM on the Flexbus and used FB_CS3 to decode it. It works better if you don't mix up your BHE and BLE strobes. With 70nsec SRAM we needed 4 wait states with a 50MHz Flexbus clock, so there is a performance penalty. You haven't specified which K60 you are using as the subfamily 3 parts will cache the SRAM and the subfamily 2 parts wont.
I don't think the MQX bit was too difficult. I think you just need to edit your .icf and rebuild your BSP.