Any example using SDHC card in FRDM-K64F through included MCUXpresso SDK SDHC module?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Any example using SDHC card in FRDM-K64F through included MCUXpresso SDK SDHC module?

Jump to solution
3,558 Views
Anonymous
Deactivated User

Hello,

FRDM-K64F board has SDHC socket already installed and wired to the SPI MCU pins. Also much promising MCUXpresso SDK has SDHC component module and board.h has macro definitions for SDHC resources. Naturally I was trying to find any example of using this module but so far failed. Any example can be found of using this provided module APIs for the microSD card operations? Logger example? or part of any demo ?

1 Solution
3 Replies
2,946 Views
Anonymous
Deactivated User

Correction: SDHC is not wired to SPI but 4 bit SDHC interface to MCU pins.

Also the FRDM-K64F SDK provided SDHC module is not the one described in MCUXpresso SDK reference manual therefore the examples provided in SDK API for Secure SD card don't work here.

0 Kudos
Reply
2,946 Views
Anonymous
Deactivated User

Thank you Mark

0 Kudos
Reply