Allowable Jitter for MK70FN1M0VMJ12 and Rise time for Reset signal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Allowable Jitter for MK70FN1M0VMJ12 and Rise time for Reset signal

1,931件の閲覧回数
puspamnayak
Contributor III


Hi,

I am using  MK70FN1M0VMJ12 in my project and using 32.768KHz Crystal, 12 MHz Crystal and 50 MHz Oscillator. So want to know if there is any limitation on Jitter or allowable jiiter for MK70FN1M0VMJ12

Secondaly want to what is the minimum/ maximum Rise time and fall time for RESET_b signals

Kindly reply soon

Thanks and Regards,

Puspam N

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,845件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

There without any jitter limitation for MK70FN1M0VMJ12 system oscillator or RTC oscillator module.

The external input clock with below requirement:

OSCILATOR.jpg

If you consider to use RESET_b pin to reset the chip, there with the minimum pulse width that is guaranteed to be recognized as a pin interrupt request.

The Min. external reset pulse width is 100ns.

There with no rise time limitation for reset_b signal.


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,845件の閲覧回数
puspamnayak
Contributor III

Hi,

Thanks for sharing the information.

Thanks and regards,

Puspam N

0 件の賞賛
返信