Add external NAND Flash to Kinetis

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Add external NAND Flash to Kinetis

1,704 次查看
luishs
Senior Contributor I

Hello.

I need add an sternal NAND Flash to Kinetis MK64 or MK66. I see these MCU do not include NFC but include Flexbus. So, its possible add a NAND Flash using Flexbus, or better I use MK60 or MK61 with NFC ?

Kind Regards

标签 (1)
2 回复数

1,471 次查看
mjbcswitzerland
Specialist V

Hi

pastedImage_1.png

FlexBus can't work directly with NAND - it would need to bit-bang various signals, making it rather inefficient.

Regards

Mark

1,471 次查看
luishs
Senior Contributor I

OK, thanks Mark.

Then best solution is use NOR Flash with Flexbus, or NOR Flash also do not need Flexbus ?.

I have check already a MICRON JS28F512M29EWHA NOR Flash, TSOP56, 512 Megas, perfect for my requirements.

I do not have experience with Flexbus, so I do not know really what's useful.

0 项奖励
回复