Add external NAND Flash to Kinetis

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Add external NAND Flash to Kinetis

1,749 Views
luishs
Senior Contributor I

Hello.

I need add an sternal NAND Flash to Kinetis MK64 or MK66. I see these MCU do not include NFC but include Flexbus. So, its possible add a NAND Flash using Flexbus, or better I use MK60 or MK61 with NFC ?

Kind Regards

Labels (1)
2 Replies

1,516 Views
mjbcswitzerland
Specialist V

Hi

pastedImage_1.png

FlexBus can't work directly with NAND - it would need to bit-bang various signals, making it rather inefficient.

Regards

Mark

1,516 Views
luishs
Senior Contributor I

OK, thanks Mark.

Then best solution is use NOR Flash with Flexbus, or NOR Flash also do not need Flexbus ?.

I have check already a MICRON JS28F512M29EWHA NOR Flash, TSOP56, 512 Megas, perfect for my requirements.

I do not have experience with Flexbus, so I do not know really what's useful.

0 Kudos
Reply