Access indivisual bits in k60 MCU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Access indivisual bits in k60 MCU

2,113 次查看
arunkumar1989
Contributor I

Hello Everyone,

This question is very basic.

I would like to know the syntax for accessing individual bits .

For example Consider this register

I2C0_C1

I would like to access the MST bit in this register.I'm not sure how to code it in code warrior.

For example in microchip's MPLAB IDE it is done like this:

I2C0_C1bits.MST = 1;     //start command

Is there any equivalent syntax in freescale cw?

I know i can OR a value to the I2C0_C1 register like this

I2C0_C1 |= I2C_C1_MST_MASK;

,but that is another alternative.

Thanks in advance,

AK

标签 (1)
0 项奖励
回复
3 回复数

2,007 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Ak,

On CW, it only can us the method you mentioned "I2C0_C1 |= I2C_C1_MST_MASK;" ,

we can see that , in the header file "MK60D10.h" , it have not define the bits of the I2C_C1 register.

And why you need use the method of "I2C0_C1bits.MST = 1;"? If it must be us the method ,you can copy the difine to the header file .


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,007 次查看
arunkumar1989
Contributor I

Hello Alice,

Thanks for the reply.Yes i figured as much.

Its not a big issue but if there was any implementation of accessing the individual bits ,it would be very help,for example i could directly return the status with a single call like this:

int myfuction()

{

     //data

     return I2C0_C1bits.MST;

}

0 项奖励
回复

2,007 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Oh Arun,

I think you can only define the bits on header file by yourself .

BR

Alice

0 项奖励
回复