About core clock deviation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About core clock deviation

ソリューションへジャンプ
1,630件の閲覧回数
zunda1958
Contributor II

Thank you for your help.


KM14 series uses SLOW CLOCK for core clock, 41.94MHz
Use as. At this time, the data sheet states that the SLOW CLOCK error is ±2%, so will the core clock also deviate like that?


thank you.

0 件の賞賛
返信
1 解決策
1,617件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Regarding the internal slow reference clock, I have checked the data sheet, the slow clock ranges from 31.25KHz to  33.4234KHz with +/-4% deviation typically, and +/-15% at most.

xiangjun_rong_0-1709711177298.pngxiangjun_rong_0-1709711177298.png

Pls check if you use internal slow or fast clock.

If you use the internal clock as core clock, of course, the core clock will deviate like the original one, but it does not take effect on the core operation.

BR

XiangJun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,618件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Regarding the internal slow reference clock, I have checked the data sheet, the slow clock ranges from 31.25KHz to  33.4234KHz with +/-4% deviation typically, and +/-15% at most.

xiangjun_rong_0-1709711177298.pngxiangjun_rong_0-1709711177298.png

Pls check if you use internal slow or fast clock.

If you use the internal clock as core clock, of course, the core clock will deviate like the original one, but it does not take effect on the core operation.

BR

XiangJun Rong

0 件の賞賛
返信