About core clock deviation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About core clock deviation

跳至解决方案
1,619 次查看
zunda1958
Contributor II

Thank you for your help.


KM14 series uses SLOW CLOCK for core clock, 41.94MHz
Use as. At this time, the data sheet states that the SLOW CLOCK error is ±2%, so will the core clock also deviate like that?


thank you.

0 项奖励
回复
1 解答
1,606 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Regarding the internal slow reference clock, I have checked the data sheet, the slow clock ranges from 31.25KHz to  33.4234KHz with +/-4% deviation typically, and +/-15% at most.

xiangjun_rong_0-1709711177298.pngxiangjun_rong_0-1709711177298.png

Pls check if you use internal slow or fast clock.

If you use the internal clock as core clock, of course, the core clock will deviate like the original one, but it does not take effect on the core operation.

BR

XiangJun Rong

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,607 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Regarding the internal slow reference clock, I have checked the data sheet, the slow clock ranges from 31.25KHz to  33.4234KHz with +/-4% deviation typically, and +/-15% at most.

xiangjun_rong_0-1709711177298.pngxiangjun_rong_0-1709711177298.png

Pls check if you use internal slow or fast clock.

If you use the internal clock as core clock, of course, the core clock will deviate like the original one, but it does not take effect on the core operation.

BR

XiangJun Rong

0 项奖励
回复