About core clock deviation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About core clock deviation

Jump to solution
1,639 Views
zunda1958
Contributor II

Thank you for your help.


KM14 series uses SLOW CLOCK for core clock, 41.94MHz
Use as. At this time, the data sheet states that the SLOW CLOCK error is ±2%, so will the core clock also deviate like that?


thank you.

0 Kudos
Reply
1 Solution
1,626 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Regarding the internal slow reference clock, I have checked the data sheet, the slow clock ranges from 31.25KHz to  33.4234KHz with +/-4% deviation typically, and +/-15% at most.

xiangjun_rong_0-1709711177298.pngxiangjun_rong_0-1709711177298.png

Pls check if you use internal slow or fast clock.

If you use the internal clock as core clock, of course, the core clock will deviate like the original one, but it does not take effect on the core operation.

BR

XiangJun Rong

View solution in original post

0 Kudos
Reply
1 Reply
1,627 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Regarding the internal slow reference clock, I have checked the data sheet, the slow clock ranges from 31.25KHz to  33.4234KHz with +/-4% deviation typically, and +/-15% at most.

xiangjun_rong_0-1709711177298.pngxiangjun_rong_0-1709711177298.png

Pls check if you use internal slow or fast clock.

If you use the internal clock as core clock, of course, the core clock will deviate like the original one, but it does not take effect on the core operation.

BR

XiangJun Rong

0 Kudos
Reply