KL02 series MCU is no LLWU module , Can i use LPTMR interrupt to reset MCU in VLLS1 mode, if it is OK, how to config ?
Also, the source code available on the website FRDM is not driven SPI modules , can i use MKL05 FRDM SPI code for MKL02?
解決済! 解決策の投稿を見る。
Hi Thooman,
Thank you very much for your focus on Freescale Kinetis product. I am glad to provide service for you.
I've had a go through the KL02's RM and it says the LPTMR interrupt can be used to generate a wakeup from any low-power mode, including the low-leakage modes.
I'd like to suggest that you can through the link below to download the FRDM-KL02's demo code which include a lowpower mode code. Wish my support can support.
http://cache.freescale.com/files/32bit/software/KL02-SC.zip
Have a nice day!!
Ping
Thanks!
I had download the source code http://cache.freescale.com/files/32bit/software/KL02-SC.zip
My problem had solved.
please see KL02 Sub-Family Reference Manual
VLLS1 only support RESET pin wakeup.
hi Thooman,
KL02 don't have Low-Leakage Wake-up Unit (LLWU) module, so you don't use LPTMR interrupt to wakeup MCU in VLLS1 mode.
Hello,
Thank you for your post, however please consider moving it to the right community place (e.g. Kinetis Microcontrollers ) to get it visible for active members.
For details please see general advice Where to post a Discussion?
Thank you for using Freescale Community.