About LPTMR to reset KL02 MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About LPTMR to reset KL02 MCU

Jump to solution
2,938 Views
thoomanwang
Contributor V

KL02 series MCU is no LLWU module , Can i use LPTMR interrupt to reset MCU in VLLS1 mode, if it is OK,  how to config ?

Also, the source code available on the website FRDM is not driven SPI modules ,  can i use MKL05 FRDM SPI code  for MKL02?

Tags (4)
0 Kudos
Reply
1 Solution
2,598 Views
xiaodong_zhang
NXP Employee
NXP Employee

please see KL02 Sub-Family Reference Manual

pastedImage_0.png

VLLS1 only support RESET pin wakeup.

View solution in original post

0 Kudos
Reply
5 Replies
2,598 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Thooman,

Thank you very much for your focus on Freescale Kinetis product. I am glad to provide service for you.

I've had a go through the KL02's RM and it says the LPTMR interrupt can be used to generate a wakeup from any low-power mode, including the low-leakage modes.

I'd like to suggest that you can through the link below to download the FRDM-KL02's demo code which include a lowpower mode code. Wish my support can support.

http://cache.freescale.com/files/32bit/software/KL02-SC.zip

Have a nice day!!

Ping

2,598 Views
thoomanwang
Contributor V

Thanks!

I had download the source code http://cache.freescale.com/files/32bit/software/KL02-SC.zip

My problem had solved.

0 Kudos
Reply
2,599 Views
xiaodong_zhang
NXP Employee
NXP Employee

please see KL02 Sub-Family Reference Manual

pastedImage_0.png

VLLS1 only support RESET pin wakeup.

0 Kudos
Reply
2,598 Views
xiaodong_zhang
NXP Employee
NXP Employee

hi Thooman,

    KL02 don't have Low-Leakage Wake-up Unit (LLWU) module, so you don't use LPTMR interrupt to wakeup MCU in VLLS1 mode.

0 Kudos
Reply
2,598 Views
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. Kinetis Microcontrollers ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 Kudos
Reply