About LPTMR to reset KL02 MCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About LPTMR to reset KL02 MCU

ソリューションへジャンプ
2,984件の閲覧回数
thoomanwang
Contributor V

KL02 series MCU is no LLWU module , Can i use LPTMR interrupt to reset MCU in VLLS1 mode, if it is OK,  how to config ?

Also, the source code available on the website FRDM is not driven SPI modules ,  can i use MKL05 FRDM SPI code  for MKL02?

ラベル(2)
タグ(4)
0 件の賞賛
返信
1 解決策
2,644件の閲覧回数
xiaodong_zhang
NXP Employee
NXP Employee

please see KL02 Sub-Family Reference Manual

pastedImage_0.png

VLLS1 only support RESET pin wakeup.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,644件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Thooman,

Thank you very much for your focus on Freescale Kinetis product. I am glad to provide service for you.

I've had a go through the KL02's RM and it says the LPTMR interrupt can be used to generate a wakeup from any low-power mode, including the low-leakage modes.

I'd like to suggest that you can through the link below to download the FRDM-KL02's demo code which include a lowpower mode code. Wish my support can support.

http://cache.freescale.com/files/32bit/software/KL02-SC.zip

Have a nice day!!

Ping

2,644件の閲覧回数
thoomanwang
Contributor V

Thanks!

I had download the source code http://cache.freescale.com/files/32bit/software/KL02-SC.zip

My problem had solved.

0 件の賞賛
返信
2,645件の閲覧回数
xiaodong_zhang
NXP Employee
NXP Employee

please see KL02 Sub-Family Reference Manual

pastedImage_0.png

VLLS1 only support RESET pin wakeup.

0 件の賞賛
返信
2,644件の閲覧回数
xiaodong_zhang
NXP Employee
NXP Employee

hi Thooman,

    KL02 don't have Low-Leakage Wake-up Unit (LLWU) module, so you don't use LPTMR interrupt to wakeup MCU in VLLS1 mode.

0 件の賞賛
返信
2,644件の閲覧回数
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. Kinetis Microcontrollers ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 件の賞賛
返信