Ability To Disable EzPort?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ability To Disable EzPort?

ソリューションへジャンプ
2,159件の閲覧回数
ee_dugan
Contributor II

Is there a way to disable the EzPort on a MK22FN128VLL10 so that it does not startup during a reset?  Our hardware can hold the EzPort CS high during reset which appears to be enabling the EzPort module?  Is there a way to disable the EzPort during programming with a configuration bit or something?

タグ(2)
0 件の賞賛
返信
1 解決策
1,943件の閲覧回数
BlackNight
NXP Employee
NXP Employee

See Disabling EzPort on NXP Kinetis to Solve Power-On Issues | MCU on Eclipse 

There is a bit (at least on K64F) in FOPT to disable EzPort.

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,944件の閲覧回数
BlackNight
NXP Employee
NXP Employee

See Disabling EzPort on NXP Kinetis to Solve Power-On Issues | MCU on Eclipse 

There is a bit (at least on K64F) in FOPT to disable EzPort.

I hope this helps,

Erich

0 件の賞賛
返信