Ability To Disable EzPort?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ability To Disable EzPort?

Jump to solution
2,149 Views
ee_dugan
Contributor II

Is there a way to disable the EzPort on a MK22FN128VLL10 so that it does not startup during a reset?  Our hardware can hold the EzPort CS high during reset which appears to be enabling the EzPort module?  Is there a way to disable the EzPort during programming with a configuration bit or something?

Tags (2)
0 Kudos
Reply
1 Solution
1,933 Views
BlackNight
NXP Employee
NXP Employee

See Disabling EzPort on NXP Kinetis to Solve Power-On Issues | MCU on Eclipse 

There is a bit (at least on K64F) in FOPT to disable EzPort.

I hope this helps,

Erich

View solution in original post

0 Kudos
Reply
1 Reply
1,934 Views
BlackNight
NXP Employee
NXP Employee

See Disabling EzPort on NXP Kinetis to Solve Power-On Issues | MCU on Eclipse 

There is a bit (at least on K64F) in FOPT to disable EzPort.

I hope this helps,

Erich

0 Kudos
Reply