AN4764 PC application source code?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AN4764 PC application source code?

8,161 次查看
frankvanhooft
Contributor III

Where can I find the source code for the little PC application in AN4764?  This thread contains a zip file with the processor source code.

AN4764 reference code

I have it running on the MKL25Z128 and it's a great little thing. I love the small size. We'd really like to make some edits to the little PC application though (for example right now it crashes if you try to connect to a board when the board's not plugged in.)  Can somebody post the source?

Thanks.

标记 (3)
17 回复数

6,938 次查看
perlam_i_au
Senior Contributor I

You can get the source code of the PC application of the AN4764 under NDA, contact your local distributor or enter a SR for more information


Have a nic day :P,
Perla

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

6,938 次查看
mjbcswitzerland
Specialist V

Hi

I have noticed that there is a (new) Windows GUI updater application in the FSL_Kinetis_Bootloader_1_0_1 package "winupdater.exe".

It looks to also allow HID uploading.

Will this one effectively replace the "HIDBootloader.exe" from AN4764? Will the HID operation nevertheless be the same/compatible?

Regards

Mark

6,938 次查看
perlam_i_au
Senior Contributor I

Yes, the FSL_Kinetis_Bootloader_1_0_1 could be a good replacement because this not only support USB HID, it also support UART, SPI, I2C or CAN.

Here is important to notice that code for appication note AN4764 and Kinetis_Bootloader are not the same.


Have a nice day,
Perla Moncada

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

6,938 次查看
mjbcswitzerland
Specialist V

Perla

Do you know whether that the HID  loader uses the same protocol in both cases?

Regards

Mark

0 项奖励
回复

6,938 次查看
perlam_i_au
Senior Contributor I

Excuse me but I did not understand, what you mean in both? both bootloaders?

0 项奖励
回复

6,938 次查看
mjbcswitzerland
Specialist V

Perla

Yes, I was asking whether the HID loading operation in KBOOT is the same as the operation used by HIDbootloader.exe (i.e. compatible) or whether it has been redesigned (uses a different set of commands etc.)

Regards

Mark

0 项奖励
回复

6,938 次查看
perlam_i_au
Senior Contributor I

As I understand these bootloaders are in fact different and each one use different methods

0 项奖励
回复

6,938 次查看
mjbcswitzerland
Specialist V

Perla

OK.- thanks.

Is there any news on next KBOOT version availability since it looks like the present version tends not to launch on Windows 7 systems and has other compatibility problems.

Regards

Mark

6,939 次查看
rogerzhong
Contributor III

The same problem occurred at my side as well. The winupdater.exe can not be launched even if Microsoft .NET Framework 4.5 has been installed correctly.

0 项奖励
回复

6,938 次查看
CCandido
Contributor V

Hi Perla,

Bootloader101, runinng with MK22FX ?

have ( Binary image boot )  there binary to be programmed?

have ( host.exe ) update binary ?

compiling error here...

thenks,

Carlos.

0 项奖励
回复

6,938 次查看
perlam_i_au
Senior Contributor I

At this moment the FSL_Kinetis_Bootloader_1_0_1 only supports the following Kinetis MCUs: K24F, K63F, K64F, KL14Z, KL15Z, KL24Z, KL25Z, KL02Z. (This is mentioned on the Bootloader page).

Regard compile error could you please share a screen print or error description?

0 项奖励
回复

6,938 次查看
mjbcswitzerland
Specialist V

Hi Perla

I have been trying to test FSL_Kinetis_1_0_1's "winupdater.exe" but it won't launch on my Windows 7 PC. I have installed the Microsoft.NET Framework 4.5 as instructed (and rebooted the PC) but it hasn't helped.

Are there any tips to make it operate?

Regards

Mark

0 项奖励
回复

6,938 次查看
CCandido
Contributor V

Hi Perla,

Microsoft.NET Framework 4.5. does not work in winXP (SP3).

how to solve?.

most of my clients still using winXP.

Framework3.5 works in winXP3.

heve solution for winXP?

thanks,

Carlos.

6,938 次查看
perlam_i_au
Senior Contributor I

On the Kinetis K64 Bootloader Quick Start Guide  is mention that this application is only supported for Microsoft .NET Framework 4.5. :smileysad:


Have a nice day,
Perla Moncada

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

6,938 次查看
EdSutter
Senior Contributor II

Hi, I'm just getting started with the FRDM-K64 board, and I've installed .NET 4.5 on my 64-bit W7 machine, but still have had no luck launching the winupdater.exe application.  Are there any other known prerequisites for this tool aside from .NET 4.5?

Has anyone run this on a W7 machine?

Thanks,

Ed

0 项奖励
回复

6,938 次查看
mjbcswitzerland
Specialist V

Ed

I can confirm that I also can't launch the program on a Windows 7 32 bit machines, with .NET 4.5 installed.

Once there is a new release I will be trying again. In the meantime there is a loader for the FRDM-K64F that allows USB HID with the original AN4764 program as well as SD card or Web server loading: https://community.freescale.com/thread/322132

Regards

Mark

0 项奖励
回复

6,938 次查看
EdSutter
Senior Contributor II

Thanks Mark,

Sure would be nice if Freescale would just open-source these tools.

Ed

0 项奖励
回复