AN2295SW fail on Compiler

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AN2295SW fail on Compiler

2,736 次查看
rabbit
Contributor III


I try to customize the bootlaoder tool for my K60 project, but the compiler fails on "Visual C++ 2008 Express Edition", here is the message:

Visual C++ 2008 Express Edition

1>------ Build started: Project: win_blsrconv, Configuration: Debug Win32 ------

1>Compiling...

1>cl : Command line warning D9035 : option 'Wp64' has been deprecated and will be removed in a future release

1>stdafx.cpp

1>c:\work\freescale\k60bootloader\an2295sw_beta\an2295\an2295sw\masters\win_blsrconv\stdafx.h(38) : fatal error C1083: Cannot open include file: 'afxwin.h': No such file or directory

1>Build log was saved at "file://c:\Work\Freescale\K60Bootloader\AN2295SW_BETA\AN2295\an2295sw\masters\win_blsrconv\Debug\BuildLog.htm"

1>win_blsrconv - 1 error(s), 1 warning(s)

========== Build: 0 succeeded, 1 failed, 0 up-to-date, 0 skipped ==========

Does anyone know how to fix it?

Regards

Sam

0 项奖励
回复
4 回复数

2,423 次查看
Gargy
NXP Employee
NXP Employee

Hello,

the issue is that the Express edition doesn't contains this file, to compile this you have to have full version.

Best regards

Petr

0 项奖励
回复

2,423 次查看
rabbit
Contributor III

Hi,

Express edition is free, the Full version cost money. Can you make one which can compile with Express version?

Reagrds

Sam

0 项奖励
回复

2,423 次查看
Gargy
NXP Employee
NXP Employee

I know,

but the whole project has long time history and it's completely build on paid version with using AFX libraries in low level of serial driver.express version -

There is no plan to switch it into Express version.

I'm sorry.

Petr 

0 项奖励
回复

2,423 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I am checking with this thread. It will take some time, I will let you know when I could get any updated info.

Thank you for the patience.

B.R.

Ma Hui

0 项奖励
回复