AN2295 protocol version 9

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AN2295 protocol version 9

ソリューションへジャンプ
7,860件の閲覧回数
Andrey
Contributor III

I'm having issues implementing AN2295 over with K70.  One of them is apparently the hc08sprg.exe does not talk protocol 9 which is defined in a target?

PROTOCOL9.PNG.png


When i hardcode it to use protocol 8 I get same a message saying "Can't read MCU info. Could be protocol error" If I open a terminal and type in "I" I get the following:

HEX_CAPTURE.PNG.png

so the mcu is talking and available. Is there a something I'm missing in the configuration of the target?

Yes, I'm using the latest app source code I was able to find, stamped with Date Modified 10/12/2012

ラベル(1)
1 解決策
7,035件の閲覧回数
pavel_krenek
NXP Employee
NXP Employee

Hi Andrey,

you are using the master application hcs08sprg version 10.0.13.0 as I see. I send you the latest one (10.0.18.0) in the attachment. Could you try it and let me know.

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
7,035件の閲覧回数
pavel_krenek
NXP Employee
NXP Employee

Hi Andrey,

you are using the master application hcs08sprg version 10.0.13.0 as I see. I send you the latest one (10.0.18.0) in the attachment. Could you try it and let me know.

0 件の賞賛
返信
4,908件の閲覧回数
RuiFaria
Contributor III

Could you share the sources of the latest one (10.0.18.0) ?

We need to build for linux platform.

 

タグ(1)
0 件の賞賛
返信
7,035件の閲覧回数
Andrey
Contributor III

Looks like that would work.

old.PNG

new.PNG

7,035件の閲覧回数
pavel_krenek
NXP Employee
NXP Employee

Hi Andrey,

I send the latest AN2295 software package in the attachment. Could you try it and let me know if there is any difference.

Regards,

Pavel

0 件の賞賛
返信
7,035件の閲覧回数
Andrey
Contributor III

Pavel,

It looks like the problem is not with the src (target) files, but with the hcs08sprg which does not recognize the new protocol for kinetis (protocol 9). I'm currently using protocol 8, and limited to 512k or so.

0 件の賞賛
返信
7,035件の閲覧回数
pavel_krenek
NXP Employee
NXP Employee

Hi Andrey,

it looks as bad trimming procedure was done. It is needed to use feature SHORT TRIM instead of break impulse which some of new serial converter cannot transfer. Try to use the windows gui and there is a check box for this feature, also you have to modify the configuration file.

Best regards,

Pavel

0 件の賞賛
返信
7,035件の閲覧回数
Andrey
Contributor III

Pavel,

I have set the SHORT TRIM settings and it still hangs.

It looks like the hc08sprog is not waiting for the complete packet. I've tried at different baud rates (9600 and 57600)

portClosing.PNG

Notice that the Close Request is done at the same instance as the Read Request

manual communication:

portManual.PNG

all the data received.

Perhaps it's a timing issue of some sort.

0 件の賞賛
返信
7,035件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Andrey,

I am checking with this issue. I will let you know when I find the way to fix the issue.

Thank you for the patience.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
7,035件の閲覧回数
Andrey
Contributor III

So it looks like I need a newer version of the PC application. Anybody has a later release than 10.0.13.0???

0 件の賞賛
返信