CADC peripheral driver in MCUXpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CADC peripheral driver in MCUXpresso

1,214 Views
SAL_111
Contributor II

I want to use the CADC driver in MCUXpresso or at least the fsl_cadc.h file to successfully initialise and do a conversion on ADCB, however I don't get this to run. Can somebody provide me an answer and explanation or an example project. I am using the MKV44F128VLF16 procesor in my project.

I am looking forward to your answers.

0 Kudos
Reply
1 Reply

1,162 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi @SAL_111,

You can use as reference the example dac_cadc from the TWR-KV46F150M SDK. 

Pablo_Ramos_0-1731357534607.png

This example demonstrates how to configure the CADC and how to read CADC values.

Hope it helps you!

 

0 Kudos
Reply