AN2295 bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AN2295 bootloader

5,173 Views
dhruvonline
Contributor III

Hi Martin,

I have a query on an2295 bootloader project posted on the forum. I am unable to open the project with IAR 7.5 version. 
Please help me in this regard.

MarMi

Regds,

Dhruv

Labels (1)
0 Kudos
Reply
7 Replies

4,682 Views
mjbcswitzerland
Specialist V

Hi

See the uTasker project for KM34: http://www.utasker.com/kinetis/TWR-KM34Z50M.html
It includes various serial loaders, including AN2295 mode: http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.pdf
which can be built with IAR, Keil, MCUXpresso, KDS, CodeWarrior, Rowley Crossworks, Greenhills, Atollic etc.

Regards

Mark

0 Kudos
Reply

4,682 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi DHRUV A,

     As I know, the AN2295 can't support the MKM34 chip, where you find the an2295 for KM34, please also share the link, I would like to help you to check it.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,682 Views
dhruvonline
Contributor III

Hi Kerry,

Here is the link. Could you please check it. 

Regds,

Dhruv

0 Kudos
Reply

4,682 Views
MehmetKirgozoglu
Contributor I

Hi DHRUVA, 

I have also been trying to find an AN2295 bootloader project example. I have found your post here but could not reach the link that you mentioned. 

Could you please share the link again? 

Thanks in advance.

0 Kudos
Reply

4,682 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi DHRUV A,

   I have use the IAR 7.80 to open it, it builds without errors.

pastedImage_1.png

pastedImage_2.png

I also tried the IAR 8.22 version, also no problem

pastedImage_3.png

pastedImage_4.png

So, you need to update your IAR version.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,682 Views
dhruvonline
Contributor III

Hi Kerry,

Thanks for the support.

I have tried with IAR 8.21. Now we are able to open the project.

But while compiling, it is giving below error. Please suggest.. 

pastedImage_1.png

Thanks&Regds,

Dhruv

0 Kudos
Reply

4,682 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi DHRUV A,

  Please check the options on your side:

pastedImage_1.png

Do you have the include directories and symbols?


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply