AHB-AP auto address increment overflow in KE04z64

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AHB-AP auto address increment overflow in KE04z64

ソリューションへジャンプ
1,636件の閲覧回数
andrewparlane2
Contributor III

I'm writing code to program a KE04z64 over SWD and am running into a few issues with the TAR register wrapping when auto increment single mode is enabled.

The ARM Debug Interface v5 doc says that auto increment is only guaranteed to operate on the bottom 10 bits of the TAR register, any more than that is implementation defined. (Specified in ARM Debug Interface v5 (IH0031A) section 8.2.2 under the Increment Single heading.

However I can't find any docs that say what this is for the KE04z64 (using the cortex m0+ core). For the K66 (using the cortex m4 core) Section 8.2.2 shows the CSW register bits, under the "Address" field, it states that the increment wraps at a 4KB boundary (so it operates on the bottom 12 bits).

I've looked in all documents I can find relating to the cortex m0+ but I just can't find any reference to this.

Any ideas.

Andrew

ラベル(1)
0 件の賞賛
返信
1 解決策
1,325件の閲覧回数
andrewparlane2
Contributor III

I've finally located this, it's in the coresight SOC TRM (which I thought I'd checked). There is a 1KB boundary which matches observed behaviour.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,326件の閲覧回数
andrewparlane2
Contributor III

I've finally located this, it's in the coresight SOC TRM (which I thought I'd checked). There is a 1KB boundary which matches observed behaviour.

0 件の賞賛
返信