ADC0_DP3 drawing more current than ADC1_SE5a

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC0_DP3 drawing more current than ADC1_SE5a

Jump to solution
1,560 Views
asfarley
Contributor IV

I'm using a FRDM-K22F with two pins configured as ADC inputs using Processor Expert. I've stuck with the default settings (longest conversion time, low-power not checked, high-speed not checked, single-ended mode, sharing not checked).

I'm testing a 5V-output sensor through a (50%) resistor divider which should give a voltage swing between 0-2.5V at the ADC input. While ADC1_SE5a seems fine (readings agree with a multimeter, etc) the ADC0_DP3 input seems to be drawing a significant amount of current, despite being configured in the same way as ADC1_SE5a. 

When the sensor is outputting 4.7V, the resistor divider gives about 2.3V through the divider if it's not connected to any ADC inputs. If I wire it to ADC1_SE5a, I still get 2.3V when sampling. If I wire the 2.3V node to ADC0_DP3, it gets pulled down to .9V. 

It appears that the resistor divider I'm using creates a sensor output impedance which is too high for the ADC0_DP3 input impedance. Why is ADC1_SE5a not having the same issues?

ADC0_DP3 gives reasonable readings using a low-impedance source (power rails or gnd) so it's not just a conversion/scaling issue. If ADC1 was sampling from more than 1 channel this could be caused by the inrush current when the channel switches but since it's only connected to 1 channel, this probably isn't the explanation. 

0 Kudos
Reply
1 Solution
1,383 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Alexander,

Please pay attation to the hardware connected to these two pins on FRDM-K22F board.

ADC1_SE5a.png

ADC0_DP3.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,384 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Alexander,

Please pay attation to the hardware connected to these two pins on FRDM-K22F board.

ADC1_SE5a.png

ADC0_DP3.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------