ADC with DMA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC with DMA

1,676 Views
ranjithshanbhag
Contributor III

Hi,@ Kerry Zhou, jeremyzhou,

Please share me example code for ADC with DMA. I did not find in example code bundle.

it will be very much helpful to proceed further.

Regards,

Ranjith

0 Kudos
Reply
3 Replies

1,492 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Could you provide the chip's part number?

There is an application note about ADC DMA application, please check here for the detailed info.

Related software could be downloaded at here.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,492 Views
ranjithshanbhag
Contributor III

Hi @ Hui_Ma

Thanks for your reply.

I am using LPC824 chip with LPCXpresso IDE.

It will be really helpful, if you provide provide sample code for above mentioned part number.

Regards,

Ranjith

0 Kudos
Reply

1,492 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Please refer attached ADC with DMA demo based on LPCXpressor54114 board, which is also suitable for LPC824 product.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply